The Power switch turns the
|
SCPI Command |
SYSTem:PDOWn NORMal|FORCe |
|
SCPI Example |
:SYST:PDOW NORM ! Executes a shutdown |
The front-panel button is not a line switch that disconnects the instrument. The power cord on the rear of the instrument must be unplugged to disconnect line power.
Restart Application (Application Shutdown)
Remote command only.
Restarts the instrument application without rebooting the instrument. Before you send this command, make sure you have saved any data that you want to preserve.
|
SCPI Command |
:SYSTem:PUP:PROCess |
|
SCPI Example |
:SYST:PUP:PROC ! You must Wait after this command for the instrument application to restart. |
|
Notes |
You cannot use *WAI or *OPC? to synchronize operation after a restart. This command stops and restarts the instrument application, thus the SCPI operation is terminated and restarted. A remote program must use a fixed wait time to resume sending commands to the instrument. The wait time will be dependent upon which applications are pre-loaded. |